Mortar Net USA Limited -

START HERE

The SpecWizard concept is simple as 1, 2, 3:
        1. Select products on the right
                by checking check boxes
        2. Configure the products
                by selecting options
        3. Generate Spec
                in Word, WP or RTF


Mortar Net USA, Ltd; masonry wall drainage systems.
.
This section is based on the products of Mortar Net USA, Ltd., which is located at:
326 Melton Rd.
Burns Harbor, IN 46304
Te1: (800) 664-6638
Phone (219) 787-5080
Fax: (219) 787-5088
Email: info@mortarnet.com
www.mortarnet.com
.
Mortar Net provides the leading solution for clogged weep holes in brick cavity construction. Featuring a patented-shaped design and 90 percent open-weave mesh, Mortar Net catches and suspends mortar droppings and other debris above the weep holes. Mortar Net prevents the mortar from forming a barrier against necessary water flow, allowing for the free migration of moisture from the wall to the weep holes.

The efficient management of moisture that Mortar Net provides eliminates efflorescence on interior and exterior masonry walls, prevents damage caused by freeze-thaw cycles, and is the first step in preventative measures that allow mold to develop, ensuring optimum performance of the walls. Mortar Net Weep Vents are used in conjunction with Mortar Net to prevent insects and debris from clogging weep holes as well as ensuring that masonry walls maintain their finished appearance.

Other products provided by the manufacturers of Mortar Net that manage water infiltration in masonry construction include Weep Vents and residential HouseNet, as well as Blok-Flash and BlockNet, which are designed for single wythe block construction.

.

Research Building Product info:
[ ARCAT.com ]

[ Comments? ]
[ What would make SpecWizard better? ]